Other Parts Discussed in Thread: OMAPL138, OMAP-L138
Tool/software: Code Composer Studio
Hi,
I refer to this 1.4.5.1.4. PDK Example and Test Project Creation.
Step1. I have installed the CCS and PDK_OMAPL138 and other components in the default path "C:\ti".As being shown below.
Step2. I create the file "MyExampleCreate.bat" in the pdk packages directory. And write "pdkProjectCreate.bat OMAPL138 all little uart all dsp" to the file.
Step3.I ran the file MyExampleCreate.bat, in the Command line window. The result is shown below.
While Copying macros.ini file, an error has occurred, as"The system cannot find the specified path".
Is there a problem with my steps?
How can I correct it?
BR.
Shide Lu.