Part Number: PROCESSOR-SDK-AM65X
Other Parts Discussed in Thread: AM6548
Tool/software: TI-RTOS
Hello,
I try to generate the example projects for the evaluation board AM6548 IDK. However, the script says that there aren't any projects.
thomas@thomas-virtual-machine:~/ti/pdk_am65xx_1_0_3/packages$ ./pdkProjectCreate.sh am65xx ========================================================================= Configuration: SOC : am65xx BOARD : all ENDIAN : little MODULE : all PROJECT_TYPE : all PROCESSOR : arm PDK_SHORT_NAME : /home/thomas/ti/pdk_am65xx_1_0_3/packages ========================================================================= Checking Configuration... PDK_PARTNO : AM65XX PDK_ECLIPSE_ID : com.ti.pdk.am65xx RTSC_PLATFORM_NAME : RTSC_TARGET : CCS_DEVICE : ***************************************************************************** Detecting all projects in PDK and importing them in the workspace /home/thomas/ti/pdk_am65xx_1_0_3/packages/MyExampleProjects No projects detected Project generation complete *****************************************************************************
I installed the recent ti-processor-sdk-rtos-am65xx-evm-05.02.00.10-Linux-x86-Install.bin
I would like to examine bare metal applications on the R5, as well as on the A53 as starting point.
Why are there no example projects for target am65xx ?
Best regards,
Thomas