Part Number: AM3358
Other Parts Discussed in Thread: UNIFLASH
Tool/software: Code Composer Studio
Hi
We are trying to burn the emmc for production , using USB boot option - RNDIS/Ethernet over USB -
and (CCS UniFlash Version: 3.4.1.00012 ) runnig over Windows 10.
The problem is the the ROM boot is able to tftp get the SPL/MLO loader butthe SPL fails to connect to uniflash
and tftp get the uboot ,You advice is needed!
See log below, Thanks.
==Log==
U-Boot SPL 2018.01-00444-g96cdbef-dirty (Feb 14 2019 - 23:19:25)
Trying to boot from USB eth
** Bad device mmc 0 **
Using default environment
<ethaddr> not set. Validating first E-fuse MAC
Could not get PHY for cpsw: addr 0
cpsw, usb_ether
Error: usb_ether address not set.
using musb-hdrc, OUT ep1out IN ep1in STATUS ep2in
MAC 38:d2:69:5e:0e:63
HOST MAC de:ad:be:ef:00:00
RNDIS ready
musb-hdrc: peripheral reset irq lost!
high speed config #2: 2 mA, Ethernet Gadget, using RNDIS
Problem booting with BOOTP
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
.