Part Number: TMDSEVM6657
Tool/software: TI C/C++ Compiler
Hello,
I need to boot from SPI NOR flash on the EVM with DDR3 initialization. I have tried this:
processors.wiki.ti.com/.../File:C6657_directROM_Boot_example.zip
However, the romparse utility crashes and the DDR3 does not read or write correctly when I use an alternate utility (bootbuild).
I am using CCS 8.2.0 and the associated pdk tools for this version.
Is there an updated set of tools that would allow me to access EVM DDR3 by booting from SPI NOR.
Thanks!
Mike