Part Number: AM4379
Tool/software: Linux
As per the SDK developer guide to rebuild the SDK without "SGX" .
after "MACHINE=am437x-evm bitbake arago-core-tisdk-image", there are the following error messages:
Summary: 4 tasks failed:
/home/user/tisdk/sources/meta-ros/recipes-extended/assimp/assimp_3.3.1.bb:do_compile
/home/user/tisdk/sources/meta-ti/recipes-kernel/linux/linux-ti-staging_4.14.bb:do_create_srcipk
/home/user/tisdk/sources/meta-qt5/recipes-qt/qt5/qtbase_git.bb:do_compile
/home/user/tisdk/sources/meta-ros/recipes-extended/pcl/pcl_1.8.0.bb:do_compile
Summary: There were 2 WARNING messages shown.
Summary: There were 5 ERROR messages shown, returning a non-zero exit code.
Need help.
Thanks and regards,
Kevin C