This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA76P: SDK_VISION RVC on HDMI

Part Number: DRA76P

 Hello Mde/Mrs

I am working on a custom board based on DRA76p , I already developed a  vision application rvc using the use case vip_single_rvc_cam_view_crc  for the ti evm baord jacinto6 witch based on dra74 and the display was on the LCD "the screen on the board" , so now  we switched to our custom board described before , I did every changes and applied the patches for this UC mentioned on the Robust_RVC-5.0_Phase-6_Release_Note.pdf , also changed the dts files and using dra76-evm-robust-rvc.dtb . but without any things can be appeared on the HDMI even in the bootloader stage !  i attached the dts files bellow .

Regards

Ahmed5127.dts_files.zip

  • Hi Ahmed,

    Can you clarify the issue for me? Is the RVC displaying on the HDMI without the changes, or is it not coming up at all after your changes for your board?

    Thanks,

    David

  • Hi David

    After all the changes there are no output over the hdmi display , the rvc didnt comming up anymore!

    the trace on remoteproc2 shows:

    0.000] 25 Resource entries at 0xa1000000
    [ 0.000] 2.758646 s: SYSTEM: System Common Init in progress !!!
    [ 0.000] 2.758890 s: SYSTEM: IPC init in progress !!!
    [ 0.000] 2.758982 s: SYSTEM: Attaching to [IPU2] ...
    [ 0.027] 2.785823 s: SYSTEM: Attaching to [IPU2] ... SUCCESS !!!
    [ 0.027] 2.785945 s: SYSTEM: Notify register to [IPU2] line 0, event 15...
    [ 0.027] 2.786067 s: SYSTEM: Notify init done !!!
    [ 0.027] 2.786311 s: SYSTEM: MsgQ init done !!!
    [ 0.027] 2.786372 s: SYSTEM: IPC init DONE !!!
    [ 0.028] 2.787561 s: SYSTEM: System Common Init Done !!!
    [ 0.029] 2.787653 s: SYSTEM: System DSP Init in progress !!!
    [ 0.029] 2.788568 s: SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1024
    [ 0.030] 2.788720 s: SYSTEM: Heap = LOCAL_L2 @ 0x00800000, Total size = 227264 B (221 KB), Free size = 227264 B (221 KB)
    [ 0.030] 2.788873 s: SYSTEM: Heap = LOCAL_DDR @ 0x00000000, Total size = 524288 B (512 KB), Free size = 522304 B (510 KB)
    [ 0.030] 2.789025 s: SYSTEM: Initializing Links !!!
    [ 0.047] 2.806441 s: SYSTEM: Initializing Links ... DONE !!!
    [ 0.047] 2.806533 s: SYSTEM: System DSP Init Done !!!
    [ 0.314] 3.072652 s: SYSTEM: CACHE: L1P = 32 KB, L1D = 32 KB, L2 = 32 KB ... after boot !!!
    [ 0.314] 3.072774 s: SYSTEM: CACHE: L1P = 32 KB, L1D = 32 KB, L2 = 32 KB ... after update by APP !!!
    [ 0.521] 3.279662 s: IPC_IN_0 : Create in progress !!!
    [ 0.521] 3.280241 s: IPC_IN_0 : Create Done !!!
    [ 0.521] 3.280516 s: ALGORITHM: Create in progress (algId = 38) !!!
    [ 0.522] 3.280790 s: ALG_drawRearview: DMA: Allocated CH (TCC) = 0 (0)
    [ 0.629] 3.388488 s: ALGORITHM: Create Done (algId = 38) !!!
    [ 0.630] 3.388793 s: IPC_OUT_0 : Create in progress !!!
    [ 0.630] 3.388977 s: IPC_OUT_0 : Create Done !!!

    Regards

  • Hi Ahmed,

    Do you mind if we close this and continue in the other thread you opened to keep it all in the same place?

    Thanks,

    David

  • Hi David,

    you can close this thread , i switched to the other one .

    Regards

    Ahmed