Other Parts Discussed in Thread: OMAP-L137
When I writting a linux kernel module to implement ARM/DSP communication, use CHIPSIG2 in SYSCFG.CHIPSIG.
I found a strange problem that my ISR of CHIPSIGINT2 got invoked 2 times though I only write a 1 to CHIPSIG.BIT[2] just once.
Here is my codes:
1. The registration of IRQ:
request_irq(irq, IRGF_RISING, dsplink_isr, "MyDSPLINK", NULL);// CHIPSIGINT2, irq=30 as in SPRUGM7D
I though maybe the irq flag is wrong, So I changed IRQF_RISING for FALLING or even 0, but that makes no difference.
2. Interrupt Service Routine:
dsplink_isr(int irq, void *dev_id)
{
......
iowrite32(1 << 2, remapped_chipsig_clr); // clear the CHIPSIGINT2 interrupt status
iowrite32(irq, remapped_aintc_sicr); // clear interrupt in ARM interrupt controller.
// or iowrite32(1 << irq, remapped_aintc_secr1); // maybe do the same thing as above.
printk("<1>ISR invoked.\n");
......
}
But always the ISR run 2 times.And if i didn't clear CHIPSIGINT2 interrupt in AINTC,the ISR will run 3 times!
I searched the BBS,and found somebody got same problem on OMAP-L137.
Could somebody point out how can I fix this problem.
PS: After ISR invoked,I checked /proc/interrupts and it appears that there is only 1 interrupt occurs, but ISR runs 2 times!
Thank you!
-- William