This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-DRA8X-TDA4X: QSGMII mode of CPSW in SDK 06.02.00 is not working

Part Number: PROCESSOR-SDK-DRA8X-TDA4X


Dear Experts:

Release Notes of SDK 06.02.00 says QSGMII mode is supported, and there is a new test case called 'CPSW9G QSGMII Switching test' in psdk_rtos_auto_j7_06_02_00_21/pdk/packages/ti/drv/cpsw/unit_test/test_framework/cpsw_testconfig.h.

I build the cpsw_unit_testapp_mcu2_0_debug.xer5f and load it through CCS, but I got no luck, the four ports on ENET EXP do not switch data packets at all, there is no packet comes from ENET EXP board.

But cable link detect is fine.

Is there any software or hardware modification required to make the QSGMII work well on ENET EXP?

Below is the UART log:

GESI board detected
QSGMII board detected

 
 ===============
 CPSW Test Select
 ===============
 
 Current/Default System Settings:
 ------------------------
 Uart timemout          : 10000 msec
 Default Iteration count            : 1
 
 1: Manual testing (select specific test case to run)
 
 s: System Settings
 
 q: Quit 
 
 Enter Choice: 
1
 
 Manual testing 

 --------------------------------------
 Select test to run as per below table:
 --------------------------------------
 
    1: CPSW9G Switching test
    2: ALE auto learn test
    3: ALE auto learn VLAN test
    4: Mac speed test
    5: Statistics test
    6: VLAN test
    8: CRC strip test
    9: FIFO stats test
   10: ALE source address update
   11: ALE Table full
   12: VLAN drop untagged
   13: Multicast support
   14: Policer test
   15: Network security test
   16: Host port Rx Filter
   17: policer no match red drop enable test 
   18: policer no match yellow drop enable test 
   19: policer no match unregulated traffic test 
   20: Intervlan test 
   21: Default priority
   22: Port VLAN ID
   23: Sanity Test
   24: Outer VLAN Test
   25: Traffic shaping Test
   26: 1-Gbps Full-Duplex Auto-Neg Test
   27: 100-Mbps Full-Duplex Auto-Neg Test
   28: 100-Mbps Half-Duplex Auto-Neg Test
   29: DMA RxFlow Mtu Test
   30: PHY Strap mode Test
   31: Priority Regeneration
   32: SGMII 1G Digital loopback
   33: SGMII 1G FIFO Loopback
   34: CPSW9G QSGMII Switching test
   35: CPSW9G All ports Switching test
   36: CPTS Event Test
   37: BCAST MCAST Rate Limit
 
 Enter Test to Run (Use UART1 console for all cores or MCU_UART1 console for MCU) 
34
34
 
 |TEST START|:: 34 ::
 |TEST NAME| :: CPSW9G QSGMII Switching test ::
 |TEST INFO| :: Num Tasks         : 1 ::
 |TEST INFO| :: Data Check        : Disabled ::
 |TEST INFO| :: Profiling         : Disabled ::
 |TEST INFO| :: Print             : Disabled ::
 |TEST INFO| :: Run Instructions  : Use QSGMII ports for switching packets ::


 |TEST ITEARATION NUMBER| ::      : 1 ::
Enabling clocks for CPSW_9G!
CPSW_9G Test on MAIN NAVSS
CpswPhy_bindDriver: PHY 16: OUI:0001c1 Model:27 Ver:00 <-> 'vsc8514' : OK
CpswPhy_bindDriver: PHY 17: OUI:0001c1 Model:27 Ver:00 <-> 'vsc8514' : OK
CpswPhy_bindDriver: PHY 18: OUI:0001c1 Model:27 Ver:00 <-> 'vsc8514' : OK
CpswPhy_bindDriver: PHY 19: OUI:0001c1 Model:27 Ver:00 <-> 'vsc8514' : OK
initQs() txFreePktInfoQ initialized with 1000 pkts
Host MAC address: 70:ff:76:1d:95:2e
PHY 16 is alive
PHY 17 is alive
PHY 18 is alive
PHY 19 is alive
Waiting for PHY link on enabled ports mask:0x72 
CpswMacPort_enablePort: SGMII Link Parter Config port 6: Link Up: 1-Gbps Full-Duplex
Cpsw_handleLinkUp: port 6: Link up: 1-Gbps Full-Duplex
MAC Port 6: link up
CpswMacPort_enablePort: SGMII Link Parter Config port 4: Link Up: 100-Mbps Full-Duplex
Cpsw_handleLinkUp: port 4: Link up: 100-Mbps Full-Duplex
MAC Port 4: link up
CpswMacPort_enablePort: SGMII Link Parter Config port 5: Link Up: 100-Mbps Full-Duplex
Cpsw_handleLinkUp: port 5: Link up: 100-Mbps Full-Duplex
MAC Port 5: link up
Waiting for PORT link on enabled ports 
CpswMacPort_enablePort: SGMII Link Parter Config port 1: Link Up: 100-Mbps Full-Duplex
Cpsw_handleLinkUp: port 1: Link up: 100-Mbps Full-Duplex
MAC Port 1: link up
Receive Complete:CpswTestCommon_recvTask,Id:0,Frame:20

U-Boot log, in case you want to know version of my EVM board

U-Boot SPL 2019.01-g350f3927b8 (Feb 17 2020 - 09:46:23 +0000)
SYSFW ABI: 2.9 (firmware rev 0x0013 '19.12.1-v2019.12a (Terrific Lla')
Trying to boot from MMC2
Loading Environment from MMC... *** Warning - No MMC card found, using default environment

Remoteproc 2 started successfully
Starting ATF on ARM64 core...

NOTICE:  BL31: v2.2(release):ti2019.05-rc1
NOTICE:  BL31: Built : 09:32:00, Feb 17 2020
I/TC: 
I/TC: OP-TEE version: ti2019.05-rc1-dev (gcc version 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36))) #1 Mon Feb 17 09:40:16 UTC 2020 aarch64
I/TC: Initialized

U-Boot SPL 2019.01-g350f3927b8 (Feb 17 2020 - 09:48:06 +0000)
Detected: J7X-BASE-CPB rev E3
Detected: J7X-GESI-EXP rev E3
Detected: J7X-VSC8514-ETH rev E2
Trying to boot from MMC2


U-Boot 2019.01-g350f3927b8 (Feb 17 2020 - 09:48:06 +0000)

SoC:   J721E PG 1.0
Model: Texas Instruments K3 J721E SoC
Board: J721EX-PM2-SOM rev E7
DRAM:  4 GiB
Flash: 0 Bytes
MMC:   sdhci@4f80000: 0, sdhci@4fb0000: 1
Loading Environment from MMC... OK
In:    serial@2800000
Out:   serial@2800000
Err:   serial@2800000
Timed out in wait_for_event: status=1000
Check if pads/pull-ups of bus are properly configured
Timed out in wait_for_bb: status=1000
Timed out in wait_for_bb: status=1000
Net:   eth0: ethernet@046000000
Hit any key to stop autoboot:  0

  • Hi Felix,

    Could you try below change in psdk_rtos_auto_j7_06_02_00_21/pdk/packages/ti/board/src/j721e_evm/board_pinmux.c?

    diff --git a/packages/ti/board/src/j721e_evm/board_pinmux.c b/packages/ti/board/src/j721e_evm/board_pinmux.c
    index dc10ebe8..f727e416 100755
    --- a/packages/ti/board/src/j721e_evm/board_pinmux.c
    +++ b/packages/ti/board/src/j721e_evm/board_pinmux.c
    @@ -431,8 +431,8 @@ Board_STATUS Board_pinmuxConfig (void)
    
             if(gBoardPinmuxCfg.gesiExp == BOARD_PINMUX_GESI_CPSW9G)
             {
    -            /* Overwrite the ICSSG RGMII muc configurations with CPSW9G RGMII */
    -            Board_pinmuxUpdate(gJ721E_MainPinmuxDataGesiCpsw9g,
    +            /* Overwrite the ICSSG RGMII mux configurations with CPSW9G RGMII/QSGMII */
    +            Board_pinmuxUpdate(gJ721E_MainPinmuxDataGesiCpsw9gQsgmii,
                                    BOARD_SOC_DOMAIN_MAIN);
                 Board_pinmuxUpdate(gJ721E_WkupPinmuxDataGesiCpsw9g,
                                    BOARD_SOC_DOMAIN_WKUP);
    

  • Hi Misael:

    I applied your patch and tried again, and the 4 ports on ENET_EXP are still not working, maybe more code modification is needed, please help me, thanks.

  • In your logs, the test appears to have completed:

    Receive Complete:CpswTestCommon_recvTask,Id:0,Frame:20

    The test stops when host port has received 20 packets, which seem to have happened here.

    What traffic are you injecting on the QSGMII ports?

  • One of my devices keep sending ARP broadcast: arping -b -I eth0 10.10.10.10

    and the rest devices monitor packets with TCPDUMP, nothing received.

    The activity LED blinks on only one port that ARP injecting, but the other ports has no activity

  • Sorry, my bad, there is some hardware problem with my EVM board, and I do the test on another EVM, QSGMII works fine.

    Thanks