Part Number: 66AK2H06
Other Parts Discussed in Thread: 66AK2H14
Hi,
This is additional question for the original post.
Customer observed overshoot/undershoot on USBCLK.
According to the original thread, USBCLK are not terminated until the software is loaded and the SERDES interface is initialized.
Customer loaded and initialized the USB module and now compliance test was passed.
But USBCLK waveform still shows overshoot/undershoot.
If customer added 100-ohm termination on USBCLK, the overshoot/undershoot disappeared.
Please see attached xls.
USB_clock.xlsx
Is this true the SERDES will apply 100-ohm termination and no termination is needed externally?
Or customer needs to setup specific register or bit to enable the internal termination?
Thanks and regards,
Koichiro Tashiro