This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6678: combining NDK_helloworld and IPC

Genius 13655 points
Part Number: TMS320C6678


Hello Champs,

Customer combined helloWorld and IPC project, please see below snapshots. 

The IPC, clock, DDR, ethernet initialization are all passed in main(). Then entering in tsk0.

 a. Core0: initializing NDK, creating UDP transmit task(priority is 5, the other tasks' priority is 1), if UDP doesn't get Tx flag, then Tasksleep->TestTask1;

b. Core1: task_yeild->TestTask1.    
                               
 TestTask1:    synchronizing core0 and core1. It will prompt error message when entering Notify() in core0. Please see below error.

Below are the code:



Thanks.
Rgds
Shine