This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748: C6748 QDMA completion status check

Part Number: TMS320C6748


I have set up QDMA to read a 16-bit port 16 times and transfer the readings to memory.  The transfer operation works as expected.  The completion of transfer is polled by checking the IPR, rather than using interrupt.  

I observed, however, that timing of other interrupts, seemingly interrupt latency is affected by QDMA.  I verified this by compiling in and out the QDMA code.  Is this expected behavior?

I perform the following before initiating QDMA:

//clear event missed status bit
HWREG(QEMCR) = 0x00000001;
//clear interrupt status
HWREG(ICR) = 0x00000001;
//clear interrupt enable
HWREG(IECR) = 0x00000001;
// trigger DMA
data_PaRAM.opt = 0x0010000C; //TCINTEN=1, STATIC=1, AB synchronization