This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-DRA8X-TDA4X: ECC implementation on TI TDA4x series

Part Number: PROCESSOR-SDK-DRA8X-TDA4X


DO TI have ECC documentation for TDA4x series ? How can i have it?

  • Vaibhav, 

    As mentioned in the earlier thread, there is no separate ECC documentation other than Chapter 12.11.4 (ECC Aggregator for MSMC) and Chapter 8.1 (MSMC); Chapter 8.2 (DDR). 

    Next level would be software examples as I mentioned in the PDK in the earlier thread. 

    jian

  • JIan,

    Yes, i have gone through chapter 8.2 and understood MSMC2DDRbridge have inline ECC support for LPDDR4. According to same tried to implement and have raised following question,

    https://e2e.ti.com/support/processors/f/791/t/925638?tisearch=e2e-sitesearch&keymatch=%20user%3A433302

    Next, i am trying to build test application which is their in PDK, but am failed to find the function implementations in PDK. 

    Thanks for support

    Vaibhav

  • Vaibhav, 

    By "function implementations" are you referring to documentation or test code? The code I referred in the PDK are at:

        \pdk_jacinto_07_00_00\packages\ti\csl\example\ecc\ecc_test_app

    you can build the test for either R5 or A53. 

    Unfortunately, documentation on CSL test programs are thin. But the source code are typically small, standalone and self-explanatory. Please give a try and let me know if you run into any build issues. 

    I will go ahead close the other two ECC threads we communicated earlier, as your now focus on MSMC and DDR. 

    regards

    Jian

  • We have build for R5 and executed the mentioned test example for DDR ECC and observed
    1. For 1 bit ECC error, interrupt is getting generated and respective handler called.
    2. For 2 bit ECC error, when test case tried to read data from test address, it generates abort instead of interrupt.
    Request you to put some pointers if above behavior for 2 bit error is correct or not.
  • Vaibhav, 

    This is the expected behavior as the double bit error was not corrected and processor would be in an unknown state and reset is required. 

    regards

    Jian