Hi,
Follow Karan's suggest. I have tried method 3 Boot App and the CAN application boot up really quickly. It handshake with vichi controller successfully.
But I meet another problem. The linux kernel start up failed. I pasted the log here.
Mcu uart print.
CAN Profile App:Variant - Pre Compile being used !!! CAN_APP: Successfully Enabled CAN Transceiver MCU MCAN0!!! CAN_APP: Successfully Enabled CAN Transceiver MCU MCAN1!!! enter can_receive_task OSPI flash left configured in Legacy SPI mode. OSPI NOR device ID: 0x5b1a, manufacturer ID: 0x2c Boot App: Started at 15612 usec Boot App: Total Num booted cores = 8 Boot App: Booted Core ID #6 at 308723 usecs Boot App: Booted Core ID #7 at 309000 usecs Boot App: Booted Core ID #8 at 320999 usecs Boot App: Booted Core ID #9 at 321274 usecs Boot App: Booted Core ID #10 at 321601 usecs Boot App: Booted Core ID #11 at 321921 usecs Boot App: Booted Core ID #12 at 322360 usecs Boot App: Booted Core ID #0 at 627022 usecs MCU Boot Task started at 15611 usecs and finished at 2174588 usecs
Main uart print - /cfs-file/__key/communityserver-discussions-components-files/791/20657.log.txt
The kernel is printing circularly.It seems some conflict with qspi. Please give me some help.
Thanks.
Regards.