This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP6713 connect to SDRAM 256Mbit



In the first contact with this DSP I made different test with the evaluation board DSK6713 and everything was fine. Right now, I've a board desing with a small differences respect to the evaluation board. One of the diference is the sdram memory that i put 256Mbit, 4 blocs, 12 row, 9 col with 32 datas. In one of the datasheets says that this memory is possible to manageted bud when i make the test doesn't work, just work if only make test until 0x10000 address. Some have the solution...

The schematics is identically to the memory of the DSK.

I apreciate your time. thank you in advance

 

Pere Cárcel