This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Sitara Processor Bring Up

I am rtrying to bring up my development board which I designed using a Sitara processor and the TPS65217b PMIC. When I give power to the board, the PMIC comes up for 50 ms, and then shuts off. It repeats this every 7.5 seconds. The micro seems to not be running, because I can see no data on UART 0. Is this normal? What do I need to do to get the system out of this mode? My design is exectly the same as the Beagle board reference design.