This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA3X EVM XGA display issue

Hi,

I have some problems with TDA3x EVM board. The doc says HDMI XGA TDM mode should be selected since VIP inputs pins is multiplexed with display output pins.

When I'm using VISION_SDK_02_06 for compiling, it all works fine. When I'm using the latest VISION_SDK_03_00, the monitor shows "out of range" when I use XGA resolution display.

In both senarios, HDMI1080p can only show two video inputs.

Is it possible to: 1. disable the multiplexed pin function that 1080p is using? or 2. find out the software change in XGA mode?

Hope to get some help from here.

Thanks,

Xing