Part Number: AM5726
When the AM572.ibs file in AM572x IBIS Model is openned , the following prompt box appears:
I don't know why ? how can I solve it ?
if you give some help , I appreciate it..
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM5726
When the AM572.ibs file in AM572x IBIS Model is openned , the following prompt box appears:
I don't know why ? how can I solve it ?
if you give some help , I appreciate it..
Hi,
Generally if errors are observed by users when loading the IBIS model it is related to the IBIS version that the tool is expecting. The IBIS model for the AM572x has been checked and is compliant with IBIS version 5.0. It will generate multiple warnings but there are no errors that have been found. Can you provide a log file which specifies the errors that are detected?
Regards, Bill
Sorry,It's very busy a few days ago. As a result of the parse file is encrypted, so I only copy the key information ,as following:
Results of the most recent parse: IBISCHK5 V5.0.3
Checking F:\Works\Simulator\IBIS\AM572x IBIS Model--2\AM572x IBIS Model\AM572.ibs for IBIS 5.0 Compatibility...
ERROR (line 6) - File_name 'AM572.ibs' contains an upper case character 'A'.
ERROR (line 6) - File_name 'AM572.ibs' contains an upper case character 'M'.
ERROR (line 859) - Model Descriptor string 'I/O_OPEN_DRAIN,1.8V,FAST MODE AND STD MODE,IND,10 PERCENT%,FAST_STD_MODE_1.8V_10P_1P8' is too long, truncating to 71 characters.
ERROR (line 860) - Model Descriptor string 'I/O_OPEN_DRAIN,3.3V,FAST MODE AND STD MODE,IND,10 PERCENT%,FAST_STD_MODE_3.3V_10P_3P3' is too long, truncating to 71 characters.
ERROR (line 861) - Model Descriptor string 'I/O_OPEN_DRAIN,1.8V,FAST MODE AND STD MODE,IND,5 PERCENT%,FAST_STD_MODE_1.8V_5P_1P8' is too long, truncating to 71 characters.
ERROR (line 862) - Model Descriptor string 'I/O_OPEN_DRAIN,3.3V,FAST MODE AND STD MODE,IND,5 PERCENT%,FAST_STD_MODE_3.3V_5P_3P3' is too long, truncating to 71 characters.
ERROR (line 1113) - Model Descriptor string 'I/O,1.8V,40D CLASS MODE FAST MODE,IND,10 PERCENT%,BC40DHHVRX_V_10P_!SC1_1P8' is too long, truncating to 71 characters.
ERROR (line 1114) - Model Descriptor string 'I/O,1.8V,40C CLASS MODE SLOW MODE,IND,10 PERCENT%,BC40DHHVRX_V_10P_SC1_1P8' is too long, truncating to 71 characters.
ERROR (line 1115) - Model Descriptor string 'I/O,1.8V,40D CLASS MODE FAST MODE,IND,5 PERCENT%,BC40DHHVRX_V_5P_!SC1_1P8' is too long, truncating to 71 characters.
ERROR (line 1116) - Model Descriptor string 'I/O,1.8V,40C CLASS MODE SLOW MODE,IND,5 PERCENT%,BC40DHHVRX_V_5P_SC1_1P8' is too long, truncating to 71 characters.
ERROR (line 1117) - Model Descriptor string 'I/O,3.3V,40D CLASS MODE FAST MODE,IND,10 PERCENT%,BC40DHHVRX_V_10P_!SC1_3P3' is too long, truncating to 71 characters.
ERROR (line 1118) - Model Descriptor string 'I/O,3.3V,40C CLASS MODE SLOW MODE,IND,10 PERCENT%,BC40DHHVRX_V_10P_SC1_3P3' is too long, truncating to 71 characters.
ERROR (line 1119) - Model Descriptor string 'I/O,3.3V,40D CLASS MODE FAST MODE,IND,5 PERCENT%,BC40DHHVRX_V_5P_!SC1_3P3' is too long, truncating to 71 characters.
ERROR (line 1120) - Model Descriptor string 'I/O,3.3V,40C CLASS MODE SLOW MODE,IND,5 PERCENT%,BC40DHHVRX_V_5P_SC1_3P3' is too long, truncating to 71 characters.
WARNING - Model Model_1: POWER Clamp : Typical value never becomes zero WARNING - Model Model_1: POWER Clamp : Minimum value never becomes zero
WARNING - Model Model_1: POWER Clamp : Maximum value never becomes zero WARNING - Model Model_2: POWER Clamp : Typical value never becomes zero
WARNING - Model Model_2: POWER Clamp : Minimum value never becomes zero WARNING - Model Model_2: POWER Clamp : Maximum value never becomes zero
WARNING - Model Model_3: POWER Clamp : Typical value never becomes zero WARNING - Model Model_3: POWER Clamp : Minimum value never becomes zero
WARNING - Model Model_3: POWER Clamp : Maximum value never becomes zero NOTE (line 2252) - Pulldown Maximum data is non-monotonic NOTE (line 2330) - Pulldown Typical data is non-monotonic
.................................
WARNING - Model Model_169: The [Rising Waveform] with [R_fixture]=50 Ohms and [V_fixture_min]=0V has MIN column DC endpoints of 0.00V and 0.73v, but an equivalent load applied to the model's I-V tables yields different voltages ( 0.00V and 0.75V), a difference of 0.02% and 3.19%, respectively.
WARNING - Model Model_168: The [Rising Waveform] with [R_fixture]=50 Ohms and [V_fixture_min]=0V has MIN column DC endpoints of -0.00V and 0.73v, but an equivalent load applied to the model's I-V tables yields different voltages ( 0.00V and 0.75V), a difference of 0.08% and 2.90%, respectively.
Errors : 14 Warnings: 1217
File Failed
Hi,
The first two errors are valid. You can fix those by changing AM572 to am572 in your IBIS model. I will change the model on the web to correct this. The rest of the errors do not appear when I run IBISCH5 v5.1.4. I think this must be a bug in the version that you are running. The IBIS5.0 spec describes the model selector statement as follows. The length of 120 characters has not been exceeded so the error should not be present.
Regards, Bill