Part Number: AM5726
Other Parts Discussed in Thread: TMS320C5517
Hi,
I am working on a voice based application where I need VOLIB and AER Libraries to be integrated with, I tested these Libraries on TMS320C5517 fixed point DSP. Now I need to implement the same on Sitara AM572x processor running on Linux. From the release information of these libraries I can find that VOLIB is supported on
| C55x/ C64x+ /C66x processors |
and AER is supported on
| 28x/55x/62x/64x/64x+/67x/67x+/674x processors |
I can also find that Sitara AM572x consist an DSP subsystem with TMS320C66x. Hence even though Sitara AM572x runs on Cortex-A15 core, since it is having C66x as DSP subsystem is it possible to use VOLIB and AER libraries along with Sitara AM572x running on linux?
Expecting a quick response, Thanks in advance.
Regards,
Janardan M