This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PROCESSOR-SDK-DRA8X-TDA4X
Hi Ti,
Can you mention steps required for booting completely from secondary media.
With steps given in "https://e2e.ti.com/support/processors/f/791/p/886980/3282433#3282433
Hi Amit,
Once you boot from eMMC. From u-boot prompt:
gpt write mmc 0 ${partitions}
The above creates a partition. Now boot to kernel using SD card.
In kernel you should be able to see /dev/mmcblk0p1
In kernel Make a ext4 fs using:
mkfs.ext4 /dev/mmcblk0p1
mkdir rootfs
mount /dev/mmcblk0p1 rootfs
Now untar tisdk-rootfs-image-j7-evm.tar.xz which is present in the filesystem folder of SDK.(Make sure you copy tisdk-rootfs-image-j7-evm.tar.xz to SD card filesystem so that you can tar that to rootfs)
cp tisdk-rootfs-image-j7-evm.tar.xz rootfs
cd rootfs
tar -xvf tisdk-rootfs-image-j7-evm.tar.xz
This should create the needed fs in eMMC.
Now get back to eMMC dip switch settings:
Your bootargs should reflect root=/dev/mmcblk0p1.
That should get rootfs from eMMC.
- Keerthy
Hi Keerthy
I followed the steps given above but i am seeing below error:
no mmc device at slot 1
SD/MMC found on device 1
libfdt fdt_check_header(): FDT_ERR_BADMAGIC
No FDT memory address configured. Please configure
the FDT address via "fdt addr <address>" command.
Aborting!
Bad Linux ARM64 Image magic!
Does this mean the uboot is not detecting emmc partition itself ?
Best regards
Amit
Amit,
Please give the full log. Which command failed and at which step.
Once you boot to u-boot prompt using eMMC.
Step 1: gpt write mmc 0 ${partitions}
Then switch back to SD boot.
As requested earlier please mention which step failed and please provide full logs for better debug.
Thanks,
Keerthy
Hi Keerthy,
1. There is no errors in any of the above command.
2. i dont understand how "gpt write mmc 0 ${partitions}" should boot from emmc. Can you explain a bit.
3. Also can you tell what is the bootcmd you use for booting from emmc.
4. If i boot from SD card i am able to see the emmc rootfs partition with the correct data.
Best regards
Amit
Hi Amit,
Please find all my answers inline.
1) That is good to hear.
2) No no that was just to create partition.
4) Nice!
3) Once you boot to u-boot prompt using eMMC boot mode do the following:
a) mmc dev 0
b) ext4ls mmc 0:1 /boot
With the above step you should see all the files in the boot folder of your eMMC filesystem that you saw in step 4.
I see something like below:
ext4ls mmc 0:1 /boot
<DIR> 4096 .
<DIR> 4096 ..
17539168 vmlinux-4.19.94-g5a23bc00e0
4250 k3-j721e-vision-apps.dtbo
3779 k3-j721e-common-proc-board-infotainment.dtbo
16933888 arago-tiny-image-j7-evm.cpio
813 k3-j721e-pcie-backplane.dtbo
<SYM> 30 vmlinux.gz
99826 k3-j721e-proc-board-tps65917.dtb
13600776 Image
101860 k3-j721e-common-proc-board.dtb
3180 k3-j721e-common-proc-board-jailhouse.dtbo
13338632 Image-4.19.94-g5a23bc00e0
7146581 vmlinux.gz-4.19.94-g5a23bc00e0
1867 k3-j721e-common-proc-board-infotainment-display-sharing.dtbo
c) Boot args:
setenv bootargs console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 vm.overcommit_ratio=5 vm.overcommit_memory=2 root=/dev/mmcblk0p1 ip=dhcp
setenv bootcmd "setenv autoload no;ext4load mmc 0:1 0x82000000 /boot/Image;ext4load mmc 0:1 0x81200000 /boot/k3-j721e-common-proc-board.dtb; booti 0x82000000 - 0x81200000"
saveenv
boot
With that you should boot Linux Prompt. I tried it myself on my J7 board.
Let me know if you are able to proceed.
Best Regards,
Keerthy
Hi Keerthy
As I do not have SD card.
Now,i can boot uboot form emmc successful.i boot kernel and dtb from tftp/nfs service(nfs mount systemfile).
Enter into system,i do mkfs.ext4 /dev/mmcblk0p1 or mount /dev/mmcblk0p1 rootfs,the system will down.
why?
Hi,
If you scroll this thread up you can see my responses.
Once you are on u-boot prompt.
gpt write mmc 0 ${partitions}
The above creates a partition. Now boot to kernel using NFS filesystem.
In kernel you should be able to see /dev/mmcblk0p1
In kernel Make a ext4 fs using:
mkfs.ext4 /dev/mmcblk0p1
mkdir rootfs
mount /dev/mmcblk0p1 rootfs
Now untar tisdk-rootfs-image-j7-evm.tar.xz which is present in the filesystem folder of SDK.(Make sure you copy tisdk-rootfs-image-j7-evm.tar.xz to SD card filesystem so that you can tar that to rootfs)
cp tisdk-rootfs-image-j7-evm.tar.xz rootfs
cd rootfs
tar -xvf tisdk-rootfs-image-j7-evm.tar.xz
This should create the needed fs in eMMC.
- Keerthy
I understand,but perhaps because mount filesystem from nfs service.As long as I do something in mmcblk0p1,the board will down