This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM437X: This project was created using a version of compiler that is not currently installed - 2.1.1 [PRU].

Part Number: PROCESSOR-SDK-AM437X

Hi,

i am using ccs9.3 in ubuntu 18.4 host.

target:AM437x-EVM

i got an error while compiling the PRU example code provided by the ti-sdk 06.03.00.106 version.

help me out.

here is the complete log:

**** Clean-only build of configuration Debug for project PRU_gpioToggle ****

/home/user/ti/ccs930/ccs/utils/bin/gmake -k clean

rm -rf "PRU_gpioToggle.hex" "PRU_gpioToggle.out"
rm -rf "PRU_gpioToggle.obj"
rm -rf "PRU_gpioToggle.d"
Finished clean

**** Build Finished ****
Buildfile generation error occurred..
This project was created using a version of compiler that is not currently installed - 2.1.1 [PRU]:
- See 'Help > Install New Software' and select 'Code Generation Tools Updates' to check if this compiler is available through a CCS update.
- Visit CCS App Center to get the latest compiler support.
- Or download and install the compiler [http://software-dl.ti.com/codegen/non-esd/downloads], then register it with CCS through 'Preferences > CCS > Build > Compilers'.
Build stopped..