Part Number: AM3358
Hello team,
I have designed a custom board using AM3358.
In one of the boards I have found that processor is not booting.I have checked the UART log and even CCCCC.... was not coming.
So, I tried connecting the board using CCS(Code Composer Studio) and found the following error.
CortxA8: Output: **** AM3358_SK Initialization is in progress ..........
CortxA8: Output: **** AM335x ALL PLL Config for OPP == OPP100 is in progress .........
CortxA8: Output: Input Clock Read from SYSBOOT[15:14]: 24MHz
CortxA8: Output: **** Going to Bypass...
CortxA8: Output: **** Bypassed, changing values...
CortxA8: Output: **** Locking ARM PLL
CortxA8: Output: **** Core Bypassed
CortxA8: Output: **** Now locking Core...
CortxA8: Output: **** Core locked
CortxA8: Output: **** DDR DPLL Bypassed
CortxA8: Output: **** DDR DPLL Locked
CortxA8: Output: **** PER DPLL Bypassed
CortxA8: Output: **** PER DPLL Locked
CortxA8: Output: **** DISP PLL Config is in progress ..........
CortxA8: Output: **** DISP PLL Config is DONE ..........
CortxA8: Output: **** AM335x ALL ADPLL Config for OPP == OPP100 is Done .........
CortxA8: Output: **** AM335x DDR3 EMIF and PHY configuration is in progress...
CortxA8: Output: EMIF PRCM is in progress .......
CortxA8: Output: EMIF PRCM Done
CortxA8: Output: DDR PHY Configuration in progress
CortxA8: Output: Waiting for VTP Ready .......
CortxA8: Output: VTP is Ready!
CortxA8: Output: DDR PHY CMD0 Register configuration is in progress .......
CortxA8: Output: DDR PHY CMD1 Register configuration is in progress .......
CortxA8: Output: DDR PHY CMD2 Register configuration is in progress .......
CortxA8: Output: DDR PHY DATA0 Register configuration is in progress .......
CortxA8: Output: DDR PHY DATA1 Register configuration is in progress .......
CortxA8: Output: Setting IO control registers.......
CortxA8: Output: EMIF Timing register configuration is in progress .......
CortxA8: Output: EMIF Timing register configuration is done .......
CortxA8: Output: PHY is READY!!
CortxA8: Output: DDR PHY Configuration done
CortxA8: Output: **** AM3358_SK Initialization is Done ******************
CortxA8: Output: **** Disabling watchdog start ******************
CortxA8: Trouble Writing Memory Block at 0x44e35048 on Page 0 of Length 0x4: (Error -1065 @ 0x3D5A) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.4.0.00006)
CortxA8: GEL: Error while executing OnTargetConnect(): Target failed to write 0x44E35048
at *((unsigned int *) (0x44E35000+0x48))=(unsigned int) 0x0000AAAA [mad.gel:284]
at Disable_Watchdog() [mad.gel:368]
at OnTargetConnect()
If I try reconnecting again without power cycling , the board is connecting and processor is ready to boot and even I could see CCCC... on the UART log.
I could sense some voltage is not being properly ramped up and is causing issue. If i am sensing correct , Kindly help me in identifying the issue and solving it.
Else let me know what could be the issue.
Kindly reply at the earliest.
Regards
Mad_hu