Part Number: AFE7950EVM
I have a AFE7950EVM connected to a TSW14J56EVM. I used the scripts in Latte to program the boards with Mode 1. I am having issues with the ADC power levels displayed on the HSDC software. The user guide mentions that the power level should be close to zero however, the fundamental signal is around -80. I have tried reprogramming the board, checking cable connections and the signal from the signal generator. I have no issues with displaying the DAC output on a spectrum analyzer however, the ADC seem to be the issue. When programming, I am not getting any unusual error messages. Any suggestions.