This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE7950EVM: DAC link breaks when capturing ADC

Part Number: AFE7950EVM
Other Parts Discussed in Thread: AFE7950

To evaluate the AFE7950EVM, I set up to step 13 according to the document "AFE7950EVM TSW14J57pptx", but if I capture with the ADC while transmitting with the DAC, the DAC link is broken and the waveform is messed up.

I want to run ADC and DAC at the same time, what should I do?

The waveform of the DAC became clear when I executed the command "AFE.adcDacSync()", but when I captured it again with the ADC, it became messy.

  • Hi Kazuto,

    This issue is expected and to solve this you should follow the Steps 6 and 7 in the AFE7950+TSW14J57 bringup guide. This consists of continuously capturing on the ADC side till the DAC output looks good, shown in step 6, then you switch ini files and and the issue no longer occurs. 

    Regards,

    David Chaparro