Other Parts Discussed in Thread: AFE7444, AFE7422
Hi,TI support,
According to the AFE7422 and AFE7444 Programmer's Guide, I failed to initialize AFE7444EVM using the SPI interface protocol.
The FPGA board I used is the ZC706 from Xilinx. I already know that when I use FMC to connect ZC706 to AFE7444EVM, I need to cut off the 5V power supply of 7444 and program the FMC interface voltage to 1.8V before burning the bit stream through Vivado.
I want to know if my operation sequence is correct, and my AFE7444EVM jumper is shown in the figure.