Other Parts Discussed in Thread: , AFE7422
Hello,TI support,
I connect zcu706 board from XILINX and AFE7444EVM to do project, when I initialize 7444 according to the AFE7422 and AFE7444 Programmer's Guide 3.1.1Start-Up GPIO Status and 3.1.2 Start-Up E-Fuse Shift, the Register Address (Hex)==0xC2,the read back Register Value (Hex) shouled be 0xF, my project cannot get this value.
I have two question:
1.when I use SPI to initialize 7444 according AFE7422 and AFE7444 Programmer's Guide,should I set the FMC voltage to 1.8V?
2.Could TI provide firmwire to initialize 7444EVM based on connecting to zcu706?
Thank you,
Wanui Hao