Other Parts Discussed in Thread: DAC39J84EVM
I have a system that will have the DAC output connected to it, and then it will provide an analog connection that I would connect to an ADC.
I don't have any test equipment other than a low BW oscilloscope so I was hoping I could just connect the DAC output of the AFE7950 to one of its ADC inputs. The main reason I selected this device is because it can do both DAC and ADC, which simplifies my setup.
In HSDC Pro, it only lets me choose the ADC or DAC tab, and the DAC tab doesn't seem to give an option to output continuously. I was hoping to set a simple tone/sine wave output, then activate the ADC and see that tone in the capture.
I was also thinking maybe this is what the FB (feedback?) channels are for?
Is any of this possible or do I have to use a separate DAC and ADC board and run two separate instances of HSDC Pro?
Also, I know next to nothing about all this JESD204 or NCO or clock setting setup stuff. I'm able to follow the guide for running Latte, but I'm using a TSW14J57 instead of the 56, and the guide is written for the 56.
Any help would be appreciated! Eventually the system under test will get a 100MSps arbitrary signal from the DAC (I'll use a predefined pattern) so I was thinking the ADC should be 500MSps, unless I can go lower by synchronizing them somehow and having the ADC sample right in the middle of the DAC samples? That's the next phase though. Right now I just want to be able to generate a DAC output and see it on the ADC input.
Thanks!