Part Number: AFE7921
Hi,
We had used AFE7921,Our usage needs
Input ref clk = 245.76MHz,input SYSREF
TX channel :4 ,RX channel :4 ,We don't use FB channel
JESD 204B lane:4 , runs 9.8304Gbps
RF Channel to serdes mask
ADC1/DAC1 – SRX/TX1
ADC2/DAC2 – SRX/TX2
ADC3/DAC3 – SRX/TX3
ADC4/DAC4 – SRX/TX4
some question about config
1.AFE7921 there are 3 sets of SPI, is SPIA used for config?
2.Regarding the sysParams.modeTdd parameter, we are going to use the FDD mode, what should this parameter be configured to?

3.If I am in TDD mode and the RX/TX 4 channels are used independently, is it configured to 0?
4.About sysParams.topLevelSystemMode I can't find a corresponding description on "AFE79xx_ConfigurationGuide_SBAA417.pdf"

5.What does this mean about sysParams.jesdSystemMode? What do the two parameters before and after the brackets mean? Also we are 4T4R, what should be the parameters?

6. About sysParams.jesdTxLaneMux and sysParams.jesdRxLaneMux,how does the lane to mux ?
Our Correspondence to ADC and serddes is below
ADC1-STX1; DAC1-SRX1
ADC2-STX2; DAC2-SRX2
ADC3-STX3; DAC3-SRX3
ADC4-STX4; DAC4-SRX4
serdes channel 5,6,7,8ia not connect

7.Regarding sysParams.LMFSHdFb, we don't use the FB channel, can just fill a random parameter in here?

8.If I want to configure other parameters,how to do it?
If we want to config sysrefTermination or serdesTxPreCursor or some other parameters.