This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38RF83: Serdes PLL lock

Part Number: DAC38RF83

There are 2 Serdes PLL lock indicators in SYSREF Alignment Circuit Alarms Register.
ALM_SD0_PLL: Driven high if the PLL in the Serdes 0 block goes out of lock.
ALM_SD1_PLL: Driven high if the PLL in the Serdes 1 block goes out of lock.

I think there is only one SerDes PLL.
What are the PLL in the Serdes 0 block and the PLL in the Serdes 1 block?

When ALM_SD1_PLL is 1 and ALM_SD0_PLL is 0, what these alarms say?
When ALM_SD1_PLL is 1 and ALM_SD0_PLL is 1, what these alarms say?