Dear Engineer,
I want to use AFE7950 to generate square wave instead of sine wave. So in the “sine_64point_att.sv” file of TI JESD 204C IP(vcu118_64b66b_2), I'm using two recurring points to replace the original 64-point sine wave. Like this:
After settig the txNco to 9GHz, I got the modulated waveform(red waveform) in the scope which shows in the first following picture. For contrast, I obtained another modulated waveform(blue waveform) by mixing the square wave generated by the arbitrary wave generator(Tektronix AWG 5208) with the carrier generated by the signal generator(Keysight EB257D).


see, the quality of waveform generated by AFE7950 is not as good as the blue waveform. The difference is mainly reflected in excessive current signal jitter and harmonic effect. Besides, the quality of spectrum is also different. Is this because the blue waveform mixed through an analog mixer?
I would like to ask what causes this signal difference and what methods can be used to improve the existing waveform generated by AFE7950.
Thanks.
Best wishes,
WANGWEI