Tool/software:
dears,
I have a customer who is using the API of AFE7921. They are trying to use API to configure AFE7921. They have the following questions:
1. Which API interfaces need to be called to configure the chip so that it can work properly?
2. Is there a complete code example available?
3. Where can I modify the working parameters? For example: NCO frequency, JESD204B configuration parameters, etc.
4. When using the API, do I need to use TI GUI to export the txt configuration file to use together?
The API version they use is CAFE79xx_V2p5.zip (zip) and the GUI version is TI-AFE79xx-Latte_V2p5.exe (exe)
Thanks!