Part Number: AFE7444
Tool/software:
Hi,
I'm using AFE7444 in mode4 with DIV3(default). I need to set the RX_A Frequency to value greater than 2.9GHz (NCO>2.9). I need to go up to RX frequency of 4.4GHz.
Can I achieve it just changing the DIV to /2?. I tried using EVM GUI to set to DIV to 2 and generate .cfg but i'm getting an error.

I manually changed the register so I can get 4423.68MHz Fadc and I can see the Fadc correctly set by probing test point. But I couldn't receive data on FPGA side if I loopback Tx to Rx.
Am I doing something wrong?


Thank you!