Part Number: AFE7950
Tool/software:
What does Table 8-5. RX Decimation Rates in the AFE7950 datasheet indicate?
Does this mean that only the sample rate listed in ADC SAMPLE LATE (MSPS) can be used?
Also, does this mean that only the decimation listed in the sample rate column can be used?
For example, is it correct to understand that a setting such as a sample rate of 2300 MHz with a decimation of 48 is not possible?