Part Number: AFE7070
I have a situation where I need to burst data into an AFE7070 from a microcontroller. I'm hoping to use Dual Input Clock Mode so that I can make use of the FIFO.
A few questions:
1. So long as I throttle using the alarm_SDO pin to avoid over-running the FIFO, can the CLK_IO be discontinuous, such that I only provide the CLK_IO when I have an I or Q data value that I want clocked into the FIFO?
2. How large is the FIFO? Please tell me if the number you quote me in I/Q pairs or in single (I or Q) entries?
3. Does the SYNC_SLEEP pin (when configured as SYNC) clear the FIFO pointers?
Thank you