Part Number: IWR1642BOOST
Other Parts Discussed in Thread: IWR1642, UNIFLASH
The goal is to reproduce a demo: http://dev.ti.com/tirex/#/?link=Software%2FmmWave%20Sensors%2FIndustrial%20Toolbox%2FLabs%2FPeople%20Counting%20Demo
The webpage indicates it is necessary to have the ES 2.0 device version:
ES2.0 devices only
This lab will only work if the IWR1642BOOST EVM has a sticker that says "ES2.0". ES2.0 devices will only work with software based on mmWave SDK version 2.0 or above. If the EVM does not have the sticker, the device is ES1.0 and requires mmWave SDK version 1.xx.xx.xx.
I would like to confirm that my device is either 1.0 or 2.0. Because I do not see a ES 2.0 sticker this link:
leads me to believe I do not have a 2.0 device. The label on the box is data rich: it's hard to tell what's what when the data field is not labeled. I am unable to find a good phone number for customer support to exchange the device. Is there a good point of contact that can assist in expediting a ES 2.0 IWR1642BOOST?