Part Number: MSPM0-SDK
This thread is used to update the software or hardware update for application note of Single Phase AC Power Monitor with MSPM0
Hardware_Software.zip
Part Number: C2000WARE Other Parts Discussed in Thread: C2000WARE , SYSCONFIG
This post is meant to specify erratas /document any refinements or clarifications discovered after the C2000Ware release.
Sysconfig migration/Switch feature in Sysconfig…
Part Number: TDA4VL-Q1 Other Parts Discussed in Thread: TDA4VL , TDA4VH
When using the MCU_ADC0 or MCU_ADC1 on TDA4VL or TDA4VH, the voltage measured on ADC0_AIN7 or ADC1_AIN7 has a higher voltage than expected (i.e., for an expected voltage of 0.8V…
This serves as a selection guide for our automotive-grade devices and outlines the typical protocols associated with these devices.
1:1
2:1
3:1
4:1
8:1
SN74LVC1G66-Q1
SN74LVC2G66-Q1
TMUX7212…
Part Number: AM625 Other Parts Discussed in Thread: AM62P , AM62L
On different TI SITARA MPU SoCs, lets have a look at SoC wise cores which have access to the OSPI module/Controller in the current MCU+ SDK Software offering. Please refer the table below…
Part Number: AM625 Other Parts Discussed in Thread: SYSCONFIG
Lets have a look at the implementation of application using a TIMER module(DM TIMER) in Interupt mode of operation.
The application code can be used as it is or as a baseline for configuring…
Part Number: AM62D-Q1 Other Parts Discussed in Thread: AUDIO-AM62D-EVM
Hi TI experts,
I am planning to reuse the AM62D-Q1 AUDIO-AM62D-EVM schematics for my custom board design. I see the below schematic sections (pages) added to the AUDIO-AM62D-EVM…
Part Number: AM6421
Hello,
During a successful QSPI boot, I have captured the following signals: MCU_PORz, RESETSTATz, OSPI_CLK, OSPI_CS. I'm observing that roughly 35mS after RESETSTATz goe high it has a 160uS period where it drops low. Looking at…