Hello guys,
One of my customers is considering using TDC7201 for their new sensor (LIDAR) unit.
They have a few questions about PWstart and PWstop parameter (Start and Stop signal pule width) as the follows.
Could you please give me your reply?
Q1. PWstart and PWstop minimum value is 10ns. But the value is longer than their achievable pulse width by the customer.
Can the minimum pulse width be reduced a little bit? For example, Is it difficult to use TDC7201 with 5ns pulse width of Start/Stop signal?
Q2. What limits this pulse width? Is it the internal ring oscillator frequency?
Or the ring oscillator clock is not used for those pulse reading and is the minimum pulse width determined
from the time which can reaches the internal circuit surely in all (Voltage, temperature and manufacturing variation) conditions?
Your reply would be much appreciated.
Best regards,
Kazuya.