Hi Experts,
Related thread is here.
There are some data formats in LongPacket such as YUV8/10, RGB888/666/565/555/444, RAW6/7/8/10/12/14, Genrric8bit, User Defined. Which format is used for AWR2243?
We assume it is RAW12 from the datasheet "Figure 9-5. Data Packet Packing Format for 12-Bit Complex Configuration". Is the same format used in case of 16 bit data?
Best regards,
Ken