Other Parts Discussed in Thread: UNIFLASH
When I test lab0012_can_sbl, receive below error:
Debug: Device info: Manufacturer: 0, Device type = 0, Capacity = 0 Debug: Loading application metaImage from Flash address: c0040000 Error: Meta header absent!!! Error: Could not download the metaimage to RAM. Trying to boot the backup factory default image. Debug: Loading backup factory default image from Flash address: c0180000 Error: Meta header absent!!! Error: Could not download the backup factory default image metaimage to RAM. Resetting the board to retry
sbl failed loading default image from Flash address: c0180000.
My question is how I can put a backup image to that Flash address. Can I use UniFlash to do that?
Kind regards