Hello,
I got no answer for last question. This is the second time I ask the same question.
I need to know how to change the number of zones in chirp config file.

I just changed zoneDef line and kept remaining file without changing.
zoneDef 21 7 10 1 14 7 10 17 14 7 10 33 14 20 10 2 11 20 10 13 11 20 10 25 11 20 10 36 11 30 10 2 11 30 10 13 11 30 10 25 11 30 10 36 11 40 10 2 11 40 10 13 11 40 10 25 11 40 10 36 11 50 10 2 11 50 10 13 11 50 10 25 11 50 10 36 11 9 10 8 32 24 10 8 32
when I run the ODDemo visualizer I got an error on command window as following.
Starting UI for Occupancy Detection Demo .... flushCfg Starting UI for Occupancy Detection Demo .... Opening configuration file chirp_configs\od_demo_18xx_8zone.cfg ... Serial port(s) already open. Re-initializing... comportnum_str = 'COM5' comportnum_str = 'COM4' Sending configuration to XWR1xxx chirp_configs\od_demo_18xx_8zone.cfg ... sensorStop Done flushCfg Done dfeDataOutputMode 1 Done channelCfg 15 5 0 Done adcCfg 2 1 Done adcbufCfg -1 0 0 1 1 Done profileCfg 0 77 250 10 40 0 0 98 1 64 2200 0 0 40 Done chirpCfg 0 0 0 0 0 0 0 1 Done chirpCfg 1 1 0 0 0 0 0 4 Done chirpCfg 2 2 0 0 0 0 0 1 Done chirpCfg 3 3 0 0 0 0 0 4 Done frameCfg 0 3 128 0 160 1 0 Done lowPower 0 1 Done guiMonitor 0 0 16 Done zoneDef 21 7 10 1 14 7 10 17 14 7 10 33 14 20 10 2 11 20 10 13 11 20 10 25 11 20 10 36 11 30 10 2 11 30 10 13 11 30 10 25 11 30 10 36 11 40 10 2 11 40 10 13 11 40 10 25 11 40 10 36 11 50 10 2 11 50 10 13 11 50 10 25 11 50 10 36 11 9 10 8 32 24 10 8 32 VODDemo:/>zoneDef 21 7 10 1 14 7 10 17 14 7 10 33 14 20 10 2 11 20 10 13 11 20 10 25 11 20 10 36 11 30 10 2 11 30 10 13 11 30 10 25 11 30 10 36 11 40 10 2 11 40 10 13 11 40 10 25 11 40 10 36 11 50 10 2 11 50 10 13 11 50 10 25 11 50 10 36 11 9 10Error: Invalid usage of the zoneDef command >>
Is there something I am missing?
Thanks,
Mostafa