Other Parts Discussed in Thread: AWR1443,
Hi Team
I would like to know the field of view of AWR1243 transciever in terms of degrees
Best Regards William
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello William,
This question has been answered by our experts in the past. Please look for some similar threads on the E2E forum.
Here is the link to one of those threads : (+) AWR1243: Which sensor for long range detection - Sensors forum - Sensors - TI E2E support forums
Regards,
Ishita
Hello Gayathri,
Let me check on the exact number internally and get back.
Regards,
Ishita
Hi,
First, it is important to understand what the Field of View is.
The FOV is the beam width at a certain db drop that can be determined from the radiation pattern
It is a property of the antenna and the sensor. The AWR1243BOOST is an evaluation board that has an AWR1243 sensor and PCB antenna.
The radiation patterns are provided in the EVM user guide in Figure 11 and Figure 12
So, for example, at 78 GHz, based on 6-dB drop in the gain as compared to bore sight, the horizontal 6dB-beamwidth is approximately ±45 degrees (see Figure 11), and elevation 6dB-beamwidth is approximately ±20 degrees
Thank you
Cesar
Thank you
Due to Summer Vacations there will no additional replies to this thread.
For new questions please start a new thread
thank you
Cesar