Hi,
This is a related question.
We did try to Implement the Idle mode commands like in Low-power example on area scanner. Now we have a few doubts
1. If the sensor is hardcoded with cfg and running and consuming the same amount of power as soon as we turn it on. Is there way to reduce the power consumption of the device while it is running without compromising with the range or performance? we do not think this command is helping me in that. Please correct me if I'm wrong.
2. We have already tried reducing the idle time on the cfg file and also the txOutPower reduced by 6 db.
3. We tried to run the bin file of the low power demo and We do not see an output or anything happening on the visualizer it just felt like the sensor is not giving out any data. Did we understand something wrong?
We can send you the exact cfg file I'm using on the sensor if it helps you to understand. We would wait to hear from you.
Regards,
Divya Teja Settimali