Other Parts Discussed in Thread: AWR6843
Hi
I have a https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/1024095/awr1843-problem-to-power-down-the-dss/3785499#3785499 thread in sensor forum, Cesar suggest me to start a new thread because TI can assign HW expert to help.
The major issue is : I use AWR1843 for a battery powered Radar, the average power consumption is about 1W not matter how I follow TI's application to tune the configure file but can not reduce too much, My goal is to reduce to 0.5W @ 250mS frame period. I try many method but can not help too much, But I find if power off the PMIC 1.0 output the current @ 5V can reduce from 280mA to 80mA, I power up the 1.0V again and restart the radar by sensorStart 0, it can work well again, but the problem is after the 1.0V power down, the MSS run very slow, seems the CPU clock speed lower than 40KHz ( originally is 200MHz ), So my question is what I can do to let the system power consumption meet my goal, for example power down BSS, DSS, or reduce the clock speed or anything that can hep?
thanks.