Other Parts Discussed in Thread: IWR6843AOP, IWR6843
Hello
I'm using IWR6843AOP evaluation board in FMCW mode for raw data capture.
Configuration is:
When looking into range-Doppler map I see 2 strong spurs at constant range bins, with varying Doppler frequencies.
from previous Questions I understand this spurs are present when crossing 59.4 GHz and 62.1 GHz, as a result of VCO nonlinearity and leakage.
and are of constant frequency (which translates to range bin, depending on slope) and non-stable Doppler. Is that correct?
Also, is it's amplitude independent of received signal amplitude?
My questions are:
1. Does using frequency band of 62.15 - 64 GHz suppose to eliminate the problem?
2. What do you mean by 59.4 GHz? Doesn't IWR6843 start at 60 GHz?
3. Why do we see it also for relatively wide bandwidth (1.7GHz)?
4. Why is it so high on AOP version? when using 'simple' IWR6843 the problem was negligible.
5. Do you plan to correct that in future versions? If so, when is that suppose to happen?
Thanks in advance,
Rakefet