This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Expert ,
Good day !
I had received some queries from the customer , please provide the help to me , Thanks
For the AWR2243 , the query are shown below :
1.I would like to know the Highest resolution at 100m range that AWR2243 Single-Chip 76- to 81-GHz FMCW Transceiver unit can achieved. We plan to use this radar AWR2243 Single-Chip 76- to 81-GHz FMCW Transceiver helping radar system monitoring a micro changing of surface shape from 100m away. It would be best that AWR2243 Single-Chip 76- to 81-GHz FMCW Transceiver will helping radar generate a no greater than 1cm resolution at 100m range.
2.do you have any other products which can fulfill the requirements list in query 1 , Can I get a product recommendation ? A TURN KEY solution is preferred ,
3. Can we have real product demonstration HD video and real life using scenario HD video?
4 .What is your recommended partner’s product that have a maximum detecting distance over 100m in different air situation and have a high resolution.
5.What are the imaging process ability for different material, for example , fire,human body, soil,plastic , steel, wood , glass?
BR,
Leon.liu
Hi Leon,
I would recommend to go thru the link below.
https://training.ti.com/mmwave-sensing-estimator-overview
I recommend using this tool for creating your initial use case based chirp configurations.
Considering your requirements as an initial tip i feel it would need a cascaded system than a single mmWave IC based sensor system.
For questions 2,3 and 4 i would request to contact local TI sales or TI RADAR marketing team.
For question 5, the solution may be a hybrid of RADAR + imaging solution for identifying the nature of obstacle.
Hi Misra ,
Thanks for your help ,
Actually , the customer do not have local TI sales agent who is responsible to their company , I think even though you send the request , some information can not be provided neither .
For the AWR2243 , I want confirm that , if the customer use the cascaded system , could fulfill their requirements (1cm resolution at 100m range) , do you have any using case or reference design can be shared to the customer ?
Same issue to the question 5.
Thanks
BR,
Leon .liu
Hi Leon,
Please refer this design for more details.
https://www.ti.com/tool/TIDEP-01012
You can refer table 1 for few more details on highest resolution.
Regards
Abhed