Hi Experts,
I am considering using the internal LDO of the AWR1843.
I have listed the following related questions, please answer.
(1) When using an internal LDO, does the LDO supply power to VIN_13RF2, VIN_13RF1, VOUT_PA?
Or is it just VOUT_PA?
(2) Currently, it is set to use LDO for evaluation. (VIN_13RF2 = VIN_13RF1 = 1.3V)
Originally, VOUT_PA should be unconnected (open), but now it is connected to 1.3V.
This is because VOUT_PA and 1.3V are connected in a board pattern and cannot be unconnected.
Is it okay to use it in this way?
(3) Even in the state of (2), it looks like it is working normally. Please tell me why it does not malfunction.
Best regards,
Jun