I'm using AWR1843 Boost.
Is VGA gain set automatically on the AWR1843 Boost?
Or is it set programmatically by the user?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm using AWR1843 Boost.
Is VGA gain set automatically on the AWR1843 Boost?
Or is it set programmatically by the user?
Hi,
Please see
https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/1036575/awr1843-about-vga-gain
Thank you
Cesar
I have a question when using mmWave Studio.
RX Gain = RF Gain + VGA Gain
I think that the formula holds, but in mmWave Studio, there is an item to set RX Gain and RF Gain Target.
I wondered, does the RX Gain item directly refer to the VGA Gain value in mmWave Studio?
Or does it represent the sum of RF Gain and VGA Gain?
Hello
Is it okay to think that in Studio the VGA is adjusted so that the difference between the RX gain value and the actually received chirp wave intensity is the VGA gain value?
After all, you can't change VGA directly in Studio, right?
I don't think so.
Let me check with design team and get back to you
thank you
Cesar
Hi,
If RX Gain is set to 24 dB and RF Gain Target is set to 30 dB, this means that RF Gain Target could be 24 and the VGA Gain 0dB in order to achieve RX Gain target. This does not mean that RF Gain will be 30dB
thank you
Cesar
Hi,
Since RF Gain Target is set to 30 dB, this means that there is enough RF gain to reach the total Rx Gain of 24dB
There is no need for gain on the VGA side
I will confirm this with design team and get back to you
thany you
Cesar
In other words, consider the case where the RF Gain Target is set to 26 dB. If you receive the RX Gain as 30 dB, the VGA Gain will be 4 dB, right? (It's bad again, but the idea is that the SDK's VGAGain sets the gain of the VGA side amplifier, isn't it?)
Hi,
As I mentioned in your other thread, this is a documentation typo. The VGA gain can't be set. We can only set the total Rx Gain and the RF Gain Target
For your example,
If we set
RF Gain Target = 26 dB
RX Gain Target = 30 dB
Thank, VGA Gain will be 4dB, you are correct
thank you
Cesar