Other Parts Discussed in Thread: MMWAVEICBOOST
Hi,
I'm trying to capture data with IWR1843BOOST, DCA1000 & mmWaveStudio. This all works, but doesn't do what I need, so I'm going to have to try to alter the s/w.
I'm downloading:
C:\ti\mmwave_sdk_03_05_00_04\firmware\radarss\xwr18xx_radarss_rprc.bin
C:\ti\mmwave_studio_02_01_01_00\rf_eval_firmware\masterss\xwr18xx_masterss.bin
> so the first question is: is the source available for 18xx_masterss, or which of the labs (e.g. OOB demo ... needs to work with IWR/DCA as above) should I use instead?
I have CCS installed and working, and can compile a lab e.g. OOB demo successfully (both mss & dss compile OK). However, when I try to debug this, I get the error:
blackhawk LAN560 emulator_0/CS_DAP_0, with text
Error initializing emulator:
(Error -2083 @ 0x0)
Unable to communicate with the debug probe. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation.
(Emulation package 9.4.0.00129)
>Is this something I've done wrong in CCS setup?
>Is there something else (s/w or h/w) I need?
>Is there some difference in the IWR setup for this? I've got the SP switches in debug mode
Modifying the s/w seems to have lots of layers - so much to learn and assimilate!
Many thanks
Alan