Hello everybody,
I am doing people counting demo using IWR6843ISK. I am saving the output of the demo. I need this for plotting is another way. My board is above 1.98m from the ground level with an elevation of 10 degrees.
So, when someone is walking the 'y' coordinate of the data should change from 0 to 5-6m as the person walk away from the board. But at about 5m the 'y' value I am getting is a maximum of 3m. Why is it so? Is there anything I should change whenever I run the demo?
Thanks in advance.
Thanks and regards,
Aleena N A