Other Parts Discussed in Thread: MMWAVEICBOOST
Hi,
I asked the wireless setup for 6843ISK previously but no ICBOOST, then I bought one. So I would like to continue the question.
The 6843ISK connects to MMWAVEICBOOST via 60Pin HD J4, and then I lost.
I would like to configure as hard-code people counting demo and transmit the data through wireless to PC via WIFI module (no embedded computer).
There are some questions:
1. The 6843ISK has been configured as hard-code. What kind of mode should I set up when I connect to ICBOOST and ISK will automatically start the sensor?
2. "connect the UART to the 40 pin header" How can I physically connect the wifi module to 40 pin header after I set the S1 as follow:
Looking forward to your reply.
Thank you.
Best Regards,
Jiaqi