Hi expert,
There are two commands adcCfg and adcbufCfg used in the mmwave sdk demo project and the parameter adcOutputFmt is used in both commands.
My questions are:
1. What is the image part? if adcOutputFmt in adcCfg is set to complex 1x and adcOutputFmt in adcbufCfg is set to 0 (complex). Is that 0 for all samples?
2. When is the complex 2x should be used preferred than complex 1x for adcCfg command.
Thinks.